Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Feedback Error States Available to MCU

All ROHM's isolated gate drivers contain undervoltage monitoring for primary and secondary. Depending on the part number, up to four outputs to the MCU allow the processor to monitor the status of the system. In addition to these signals, some also include an isolated temperature monitor permitting indirect measurement of the power device base plate or chill plate temperature.

PTM Veröffentlicht am: