Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Reed Switch Magnet Interaction Slide 18

The magnet is parallel to the reed switch with the three lobes of magnetic sensitivity arrays. The magnet is placed in the middle of the center lobe and centered over the reed switch contacts. In this case it is known that since the magnet is within the Pull-in lobe the contacts will be closed. The magnet will now be rotated about its axis by 90°.

PTM Veröffentlicht am: