Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Reed Switch Magnet Interaction Slide 23

When viewed in three dimensions, the magnetic flux lines emanating from the magnet look like a beer barrel keg. With the magnet parallel to the reed switch, the center magnetic lobe array looks like a donut and the two outside lobes look more like a boxer’s punching bag, the kind hung from the ceiling. Essentially the fields from the magnet and the fields for the lobes are symmetrical when viewed in three dimensions. As seen in two dimensions, when the magnet is brought into one of the lobes the reed switch contacts will close. Now, as seen in three dimensions the magnet can be brought into the lobes in any spherical direction for contact closure to occur.

PTM Veröffentlicht am: