Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Reed Switch Magnet Interaction Slide 20

With the magnet parallel to the reed switch the three lobes are present showing the generated arrays of magnetic sensitivity. The magnet is positioned within the pull-in lobe, so that ordinarily this position would close the contacts; however, in this case a magnetic shunt is positioned between the magnet and the reed switch. The magnetic shunt is comprised of a ferromagnetic material – nickel, iron or cobalt. In this case, the magnetic sensitivity lobes remain the same, but the magnetic flux lines emanating from the magnet travel almost entirely within the magnetic shunt instead of through the reed switch. Without the magnetic flux lines traveling through the reed switch, the contacts will remain open.

PTM Veröffentlicht am: