Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Reed Switch Magnet Interaction Slide 19

Rotating the magnet from parallel to perpendicular will cause the contacts to go from a closed state to an open state. If one continued to rotate the magnet the contacts would open and close after each 90° rotation. Many applications use this approach to count rotations of mechanisms that in turn translate the rotations to specific functions. One common application is in water filters. As the water flows a magnet is rotated. Counting the rotations allows one to keep track of the amount of water filtered, eventually indicating it’s time to change the filter.

PTM Veröffentlicht am: