Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Reed Switch Magnet Interaction Slide 3

A reed switch is a small electromechanical device generally having two ferromagnetic leads that are separated internally in a hermetically sealed glass envelope. When the reed switch, which comes in various sizes, is brought into a magnetic field, the reed leads will close creating a switching function. Closing the reed contacts takes a certain magnetic strength measured in milli-Tesla (mT) or ampere turns (AT). This is called the pull-in point (PI). When removing the magnet the contacts will open at some point. This is called the drop-out point (DO). Hysteresis is another useful parameter, it is the ratio of the pull-in divided by drop-out (PI/DO). Ferromagnetic materials are materials that become magnetized when they enter or are influenced by a magnetic field. Iron, nickel, and cobalt are the most common ferromagnetic materials.

PTM Veröffentlicht am: