Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Secondary Side Switch-Mode Power Supply Control Slide 10

On this slide, ST’s Constant Current/Constant Voltage roadmap shows some of the applications on the vertical axis such as notebook power supplies, adapters, chargers, slim PCs, gaming consoles, and all sorts of digital video products, as well as mobile phones. Along the horizontal axis the release date timeline is shown. The various package types such as SO8, Micro SO8, and SOT23-6L can be seen. There are some new products shown, the SEA01, which has digital trimming capabilities as opposed to trimming it by using resistors. Also shown is the SEA05L which has additional features that will be discussed later in the presentation. Additionally, STMicroelectronics offers devices with low power consumption which is important for adaptors where the goal is to maintain the lowest possible no-load power consumption.

PTM Veröffentlicht am: