Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Secondary Side Switch-Mode Power Supply Control Slide 6

For constant current/constant voltage secondary side control, ST has an integrated solution available for use in switch-mode power supplies that require both precise constant current and constant voltage regulation for battery chargers and adapters. The TSM1013 is one example of a device that could be used for this. It can be seen on this slide that this device has an integrated precision voltage reference for Vref and also an op-amp for current control and another op-amp for voltage control. The inputs and outputs for each the op-amps are all brought out on the IC pins.

PTM Veröffentlicht am: