Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Secondary Side Switch-Mode Power Supply Control Slide 34

In summary, STMicroelectronics has an integrated solution available for use in for CC/CV secondary side control for switch-mode power supplies for battery chargers and adapters. The TSM1013 is an example of a device that could be used in this type of application. Precise secondary side current control and voltage control loops make a more robust design possible by using Constant Current/Constant Voltage ICs. Synchronous rectification is used to increase power supply efficiency by reducing the losses associated with output rectification. SR replaces the typical Schottky rectifier with a MOSFET for the output rectification, this results in lower power losses. Examples of applications using the ST PM8834 to drive synchronous rectification MOSFETs are DC/DC bricks and telecom, or a PFC boost MOSFET in a large power supply.

PTM Veröffentlicht am: