Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Secondary Side Switch-Mode Power Supply Control Slide 12

The TSM1052 is a new device for CV/CC controller for SMPS applications. It is an evolution of the TSM1051 as was mentioned on the previous slide. It has a wider operating range, as well as a lower input voltage which makes it more useful for lower voltage output applications. The device increases the robustness for safe startup and accidental feedback disconnection, so if the feedback is lost for any reason it will not destroy itself. In addition, lower power consumption is based on the supply quiescent current of 150 µA, which helps for the energy saving regulations for adapters and other products that require low power consumption.

PTM Veröffentlicht am: