Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 33

This slide shows the vertical parameters, from the minimum to the maximum, and includes overshoot and undershoot. The amplitude is measured from the base to the top, and does not include overshoot and undershoot. When measuring rise time, for example, it will be measured from 10% to 90% of the rising edge, and fall time is measured from the 90% to 10% of the falling edge. There are also user definable levels which allow the user to measure rise and fall time in any desired portion of the waveform.

PTM Veröffentlicht am: