Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 47

Looking at the effects of frequency on probe impedance, when a typical 10 MΩ probe is used at low frequency the input resistance is dominant, but as the frequency increases the input capacitance becomes dominant. Typically, a passive probe is going to measure somewhere between 9 pF and 12 pF of capacitance. A possible result is that the capacitive loading effect changes the form of the signal of interest, so the user is not getting a true representation of the waveform.

PTM Veröffentlicht am: