Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 9

This slide illustrates the use of real time sampling. The waveform at the top is a very narrow sinusoidal signal. The Nyquist theorem specifies sampling this at a minimum of 2x the frequency of interest. In this example it can be seen that the sine wave is sampled with five sample points and then the reconstructed wave form is shown on the screen. Pulse and square wave type wave forms are very broadband, and are extremely rich in harmonics. These must be sampled typically ten times. The lower illustration shows that when dealing with pulses and square waves more sampling points are required to reconstruct the wave form. This is where the digital bandwidth of the scope comes into play, offering enough memory and a high enough sampling rate to capture the true shape of the signal.

PTM Veröffentlicht am: