Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 8

Several types of sampling techniques are shown on this slide. Real time sampling is the default mode in most oscilloscopes. It is very good for capturing transient signals, depending on the time base and the number of channels being interleaved, or not. One problem to consider is that it might exhibit problems of aliasing which will be discussed later. Random interleave sampling, also called Equivalent Time Sampling does multiple sampling. It is only to be used for repetitive signals not transients, but it gives a higher effective sample rate. For very low frequency phenomena a good selection is the roll mode.

PTM Veröffentlicht am: