Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 6

Shown on this slide is a Bodi plot example for a 600 MHz oscilloscope, where the 3 dB point is .707 of the input. This would be a typical response curve of a 600 MHz oscilloscope. Adding a passive probe, which typically has a bandwidth of 500 MHz, it can be seen that the response curve rolls off a little quicker, before 600 MHz. Adding an active probe, which will be discussed in more detail, the bandwidth of the system is extended to beyond the 600 MHz. Therefore, when using the active probe the system bandwidth is guaranteed to be 600 MHz.

PTM Veröffentlicht am: