Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
MAX V Overview Slide 13

No programmable logic solution is complete without software tools. The MAX® series of CPLDs are backed by one of the easiest to use tools in the industry, Quartus® II. There is no need to learn another tool set to use CPLDs; Intel® CPLDs use the same tools as the Intel® FPGAs and HardCopy ASICs. Intel® offers many MegaCore applications that make designing quick and easy. MegaCore examples include the parallel Flash Loader used to program FPGAs from parallel Flash Memory, a full library of the familiar 74-Series of components, and the In-System Sources and Probes editor which allows the addition of Quartus® II controlled real time debugging. The MAX® Series CPLDs and the IP are included in the Free Quartus® II Web Edition Software. Download this software now by clicking on the URL link at the bottom of the page.

PTM Veröffentlicht am: