Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
MAX V Overview Slide 17

Shown in the block diagram on this slide is how a MAX® V CPLD may be used to provide I/O expansion and decoding for an ASSP. In this application the MAX® V CPLD can be used to add extra GPIOs, interrupt sources, PWM outputs, chip select decode and/or flash key or serial-ID storage, analog light level input using LED, with I²C used to connect to GPIOs, interrupts, PWM, and light sensor. Additionally, the MAX® V CPLD is being used to generate additional chip select outputs from the DFI or EBI2 address lines.

PTM Veröffentlicht am: