Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
MAX V Overview Slide 18

The diagram on this slide shows how MAX® V can also control many other power supplies through enabling LDO regulators, controlled by multiple MOSFETs. With this approach, the only parts of the system actually in use are powered up and those not being used are powered down to maximize battery life or to keep system power as low as possible.

PTM Veröffentlicht am: