Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Film-Cap-Slide11
The B3202x series varies up to 1µF with a Y2 safety classification, 300 VAC rated voltage, and 100ºC temperature range. Note that 300 VAC is the maximum rating allowed by IEC for Y2. In the event that a higher safety requirement is requested, the X1 EPCOS series (with 4 kV impulse test), can also be used. There are two series: one rated at 330 VAC up to 6.8µF, and other rated at 440 VAC up to 1µF.
PTM Veröffentlicht am: