Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Film-Cap-Slide4
Film capacitors have a self-healing capability and can clear faults in the film such as pores or impurities while under a voltage. The metal coatings, vacuum-deposited directly onto the plastic film, are only 20nm to 50nm thick. A dielectric breakdown occurs when the field strength is exceeded locally at a weak point. The high temperatures reached (up to 6000K) in the breakdown channel transform the dielectric into a highly compressed plasma that forces its way out.
PTM Veröffentlicht am: