Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Slide11

A ball bearing is a type of rolling element bearing that uses balls to maintain the separation between the moving parts of the bearing. The purpose of a ball bearing is to reduce rotational friction and support radial and axial loads. The bearing achieves this by using at least two races to contain the balls and transmit the loads through the balls. Usually one of the races is held fixed. As one of the bearing races rotates it causes the balls to rotate as well. Because the balls are rolling they have a much lower coefficient of friction than if two flat surfaces were rotating on each other. Ball bearings tend to have lower load capacity for their size than other kinds of rolling element bearings due to the smaller contact area between the balls and races. However, they can tolerate some misalignment of the inner and outer races. Compared to other rolling element bearings, the ball bearing is the least expensive, primarily because of the low cost of producing the balls used in the bearing.

PTM Veröffentlicht am: