Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Slide21

Thermal protection is a method of fan motor protection that is activated when a fan motor locks up with the power still being supplied. It uses a thermal relay inside the motor to break the circuit to the winding coil without causing damage. A thermal relay is connected in series with the coil and operates by detecting the temperature of the winding coil. Ordinarily, thermal protection is used for large fans that cannot be sufficiently protected by impedance protection.

PTM Veröffentlicht am: