Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Slide19

DC brushless motors run cooler than AC motors, have more precise control, and higher torque levels. The DC motor typically operates within an efficiency range of 85%-90%. The components that make up a DC brushless motor are the stator with windings, permanent magnets on the rotor, an external electronic switch synchronized to the rotor.

PTM Veröffentlicht am: