Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Slide5

If the fan blades are very close to a structure which is not symmetric, unsteady interaction forces on the blades are generated which causes noise to occur. Impulsive noise is caused by the interaction between a blade and the blade-tip-vortex of the preceding blade. This type of noise is not severe in cooling fans but it can occur. Asymmetry of the rotor causes noise at the rotating frequency and it’s harmonics, even when the inlet flow is uniform and steady.

PTM Veröffentlicht am: