Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Slide9

Fan size is typically one of the top specifications in determining if a certain fan will work for a particular application. The example on this slide is an excerpt from Qualtek’s 120 mm x 38 mm fan specification sheets which shows the thickness, height and width of the fan as well as the size of the mounting holes. By combining all of this information into one easy to read location, finding the right fan is much easier.

PTM Veröffentlicht am: