Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Slide16

Qualtek uses two types of AC motors in its AC axial fans. These two types are shaded pole and permanent split capacitor. The shaded pole type of motors are very inexpensive to produce at the  cost of having low starting torque and low efficiency, but are extremely rugged. Permanent split capacitor motors are more expensive than shaded pole motors and feature the benefits of having improved starting torque and a large increase in efficiency.  The next two slides will further discuss each motor type in more detail.

PTM Veröffentlicht am: