Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 11
The Si1102/Si1120 should be placed as close to the window as possible in the design. If the Si1102/Si1120 are deeply recessed into the product enclosure, it will require a convex lens with a focal length equal to the distance from the window to the detector to collect light in the axial direction. The larger the hole, the better the light collection. Please keep in mind that lenses are not recommended for IR slider applications.
PTM Veröffentlicht am: