Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 13
Shown here are the key features of the Si1120 which integrates all of the analog features required to implement robust IR proximity detection as well as ambient light sensing in a single package. The Si1120 provides a single pulse PWM output that is easily measured with an MCU and provides low power operation. Upcoming slides will show how to configure the Si1120 and take proximity measurements with a sample application.
PTM Veröffentlicht am: