Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 6
Illuminance is the total luminous flux (the flux density corrected for human vision) in a given area. The table above is provided in order to get an idea of how ambient light relates to real world environments by comparing the illuminance values for each. It can be seen from this table that proximity sensing applications are required to compensate for a wide range of ambient light conditions. As mentioned earlier, these values represent the visible spectrum. There are IR components that are part of the entire radiant flux in the environment that can interfere with the proximity measurements.
PTM Veröffentlicht am: