Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 27
There is an evaluation board from Silicon Labs which includes seven LEDs. The evaluation kit is able to implement several measurement modes including: single proximity measurements, three LED motion measurements, two LED slider measurements and ambient light sensing. The kit provides interface to the C8051F930 low power MCU and highlights the time division multiplex scheme for monitoring multiple LEDs. Additionally, it interfaces to the QuickSense Studio GUI.
PTM Veröffentlicht am: