Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 30
The Si1102 Evaluation Kit (Si1102EK) is an additional tool from Silicon Labs. It offers infrared threshold detection where a visible LED illuminates when an object crosses an invisible threshold. The Si1102EK offers a configurable range where the proximity threshold range and scan rate is controlled by two thumb-wheel potentiometers. This evaluation kit is operated by a single coin-cell battery, no external power is required. Contents of the kit include the Si1102AB demo board and the Si1102EK Quick Start Guide.
PTM Veröffentlicht am: