Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Power over Ethernet Slide 11
In the above diagram, the PSE (Power Sourcing Equipment) is the PoE device and the PD, powered device (mode B), is the application. For a compliant power supply, on the left hand side, this diagram shows a non-PSE switcher hub, which simply provides data over the lines. The PSE is the actual power supply. Data is passed through the power supply but the unit also provides power over the unused pairs to the end station or the PD.
PTM Veröffentlicht am: