Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Power over Ethernet Slide 17
The goal for the new standard - expected to be ratified in 2008 - is to increase the maximum power rating from the 15 to 20 watt range to the 30 to 60 watt range. This will provide greater power for evolving applications such as motorized network cameras, IP telephony videophones, RFID readers, access-control systems, point-of-sale, information kiosks and laptops. Also, the 802.3at standard will allow backward compatibility for 10, 100, and 1000 Base T applications.
PTM Veröffentlicht am: