Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Power over Ethernet Slide 5
There are two modes, A and B, of PoE available. In mode A, pins 1 and 2 form one side of the 48 volt DC supply, and pins 3 and 6 provide the 48 V return. These are the same two pairs used for data transmission in 10Base-T and 100Base-TX, allowing the provision of both power and data over only two pairs in such networks. In mode B (most common and shown in the figure above), pins 4 and 5 form one side of the DC supply and pins 7 and 8 provide the return; these are the "spare" pairs in 10BASE-T and 100BASE-TX. Mode B, therefore, requires a 4-pair cable.
PTM Veröffentlicht am: