Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Power over Ethernet Slide 25
How much power will the PD device require? There are two power levels based on the standard used. The 802.3af is 15.4 watts. The 802.3at will be 30 to 60 watts. It is important to understand what the application is and how much power is required so the best solution is found.
PTM Veröffentlicht am: