Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Power over Ethernet Slide 8
A PD will determine which mode of PD is connected, mode A or mode B, and may also classify its power requirements. After the PSE has discovered a PD, it supplies 48V and a maximum current of 350 mA. Voltage may be lost along the cable, depending on distance. However, a minimum of 13 watts is available to each PD.
PTM Veröffentlicht am: