Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Power over Ethernet Slide 7
In the 802.3af standard, devices within the power supply allow it to ramp up to the proper voltage. For example, the power supply looks for a proper capacitive or resistive signature and if detected, it ramps up to four volts. The process is repeated by checking for the signature again. If detected and there are no faults, the power supply ramps up to eight volts. The process is repeated one more time and if the proper signature is again found, it will ramp up to the full forty-eight volts to power the system.
PTM Veröffentlicht am: