Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Reed Relay Overview Slide 10

Shown on this slide is the pattern across the contacts shortly after the reed switch contacts close. To initiate this action, a voltage is applied to the coil shown at time 0.0. The area highlighted in gray represents the time after the voltage was applied to when the contacts make their first closure. In the case shown it takes about 0.25 ms. The contact bounce is highlighted in blue. In this case the contacts have one bounce, in which the contacts open completely before reclosing.

PTM Veröffentlicht am: