Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Reed Relay Overview Slide 22

Other automatic test equipment with reed relays usage are: cable testers, discrete semiconductor testers, power component testers and more. With more than 20,000 switching points, the switching devices must be extremely small. It is not unusual to have up to 30 layers making up the printed circuit boards that will house these switching points, with switches mounted on both sides of the boards. These boards are very expensive, driving up the cost of real estate on the boards. Reed relay manufacturers have been able to meet this challenge by offering very small reed relays in a surface mounted package.

PTM Veröffentlicht am: