Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Reed Relay Overview Slide 7

As can be seen on this slide, with the closure of the contacts there is a slight vertical motion, as well as a horizontal motion. This results in a scrubbing action on the contacts. This movement is occurring hundreds of times per second. Any non-uniformity on the contact surfaces, or particles, will present a different frequency pattern. If there are any slight cracks, or stress to the reed switch, the frequency patterns will also be altered.

PTM Veröffentlicht am: