Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Reed Relay Overview Slide 5

The breakdown voltage is the voltage that the contacts are capable of withstanding where no breakdown or arc-over will occur. The insulation resistance is the resistance across the contacts and/or the resistance between the coil and the contacts. For a reed relay it is typically as high as 10 TΩ (1 with 13 zeros following it). Common reed relay applications can require many tens of millions of switching operations. Testing the contacts dynamically is critical to determine if there are any tiny flaws in the reed switch which can result in early life failures. This is a very important parameter for long, reliable, reed relay life.

PTM Veröffentlicht am: