Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Overview-Slide20

Additionally, many intelligent peripheral features are provided that allow tasks to be completed independent of the CPU and far more efficiently. These include the autoscan feature in the ADC12 and the available DMA. With the intelligent peripherals, the CPU does not need to be over clocked to deliver the required system performance. One final precaution, always review manufacturers worst case or maximum values over all operating conditions as many specifications are dramatically effected by temperature.

PTM Veröffentlicht am: