Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Overview-Slide31

From the first day of development, firmware engineers can now unobtrusively develop and debug their embedded code with full-speed execution, breakpoints, and single steps in an application. Embedded emulation becomes even more important with high performance mixed-signal systems that must maintain the integrity of microvolt analog signals. Signal integrity is virtually impossible with cumbersome in-circuit emulators that are sensitive to cabling crosstalk. Also, unlike abstract background debuggers, no time-sharing of system serial communication resources is required with the embedded emulation on the MSP430.

PTM Veröffentlicht am: