Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM3U Cortex-M3 Based MCU Introduction Slide 13
There are two bridges on the SAM3U: one for low-speed peripherals with Peripheral DMA Controller (PDC) support, and one for high-speed peripherals with central DMA support (SSC, HSMCI and SPI). The two different bridges mean two different slaves on the system, which allow fetch from the internal SRAM or internal Flash and at the same time perform a transfer from the MMC to MC card or SD card. Thanks to the 5-layer bus matrix, the user is able to parallelize different transfers and thus can connect five different masters to up to ten different slaves.
PTM Veröffentlicht am: