Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM3U Cortex-M3 Based MCU Introduction Slide 9
As a review of the previous slides, this slide lists the major points of the implementation of the Cortex-M3 on the SAM3U: the Cortex-M3 Revision 2 is embedded; clock gating to reduce power consumption in low-power modes is implemented; Memory Protection Unit is embedded; NVIC is implemented, without NMI, but providing thirty interrupts and sixteen priority levels. Debug level 3 and Trace Level 1 have been implemented; and there is no implementation of the Wakeup Interrupt Controller as the same feature is handled by the Supply Controller of the SAM3U.
PTM Veröffentlicht am: