Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM3U Cortex-M3 Based MCU Introduction Slide 8
The Cortex-M3 is configured by default in JTAG mode. But the SAM3U also supports the Serial Wire Debug (SWD) mode which reduces the number of pins dedicated for debug. Only two are necessary: SWCLK and SWDIO. An extra one called TRACESWO is dedicated to the Asynchronous Trace (ITM) feature that is also supported. Serial Wire Debug mode as well as Asynchronous Trace (ITM) are both supported by the JTAG SAM-ICE. The table on this slide shows the different pins which are used in JTAG and in Serial Wire and Asynchronous Trace.
PTM Veröffentlicht am: