Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM3U Cortex-M3 Based MCU Introduction Slide 19
The SAM3U evaluation board has three devices connected to the External Bus interface: a color QVGA TFT with resistive touchscreen, a 2 Gigabit NAND Flash and a 1 MegaByte 16-bit pseudo-static RAM. It also has a high-speed SDCard/SDIO/MMC interface, standard audio line-in, headphone and microphone connectors, two ADC inputs, one for the 12-bit and one for the 10-bit ADC, a 3D accelerometer sensor and several standard serial, USB and JTAG ports.
PTM Veröffentlicht am: