Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM3U Cortex-M3 Based MCU Introduction Slide 18
An outstanding feature on the SAM3U4 is the dual-boot Flash bank selection capability for IAP. This is managed by one of the GPNVM bits. GPNVM bits 0 and 1 have the same functionality as on the SAM7 products, but the GPNVM bit 2 is specific to the SAM3U. This bit is responsible for the Flash selection, either Flash 0 or Flash 1. There are two Flash banks available, Flash bank 0 at the address 80000 and Flash bank 1 at address 100000. The user may have two different applications. When the GPNVM bit 2 is cleared, boot will occur at Application 1, and the Application 1 will be seen at Address 0. If the GPNVM bit 2 is set, then boot will occur at Application 2, or the Flash Bank 1 seen at Address 1. This is particularly useful when the customer wants to perform In-Application Programming.
PTM Veröffentlicht am: