Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM3U Cortex-M3 Based MCU Introduction Slide 7
The Cortex-M3 used in the SAM3U has six code breakpoints and four general-purpose watchpoints, providing enough breakpoints for most cases of debugging. There are two debug interfaces, the JTAG and the Serial Wire. The serial wire is a 2-pin debug interface which enables asynchronous traces (data traces and profiling). The Cortex-M3 also allows live access to the core when the application is running, making it possible to read and write memory and to set or clear breakpoints on a running application.
PTM Veröffentlicht am: