Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
cable jackets
Cable jackets provide additional chemical, mechanical, and environmental protection. Jackets also make cable installation easier by bundling many individual conductors together.  A cable jacket may be applied directly over the insulated conductors or as a core wrap over the shield. There are many different jacket materials used depending on the application of the cable. Different jacket materials will be used on cables for indoor applications that need to meet certain electrical codes or standards. Galvanized steel or aluminum are the most popular metals used for this type of armor.
PTM Veröffentlicht am: